Serial_Interface_Parameters
Serial_Interface_Parameters
| Address: | -- | ||||||||||||||||
| Type: | WORD | ||||||||||||||||
| Access: | Read/Write | ||||||||||||||||
| Unit: | -- | ||||||||||||||||
| Range: |
0 to 258 Serial Data Format
Modbus DWORD Order
|
||||||||||||||||
| Default Value: | 0 | ||||||||||||||||
| Store Supported: | No | ||||||||||||||||
| Description: |
This object is used to change the settings of the Serial Communication Interface. This object can be changed only inside the user's application and it's execution is dependent to the status of U0 dip (see §Baud Rate & Node Id Selection for Drives). If U0 dip is OFF the execution of this object is not allowed and it will not change the standard settings of the Serial Communication Interface. The U0 dip must be ON to allow the working of this object. For drives not fitted with dips-switches or rotoswitches this objects is always executed. The Service Serial Communication interface is not affected by the value of this object. |
||||||||||||||||
| Notes: | The Kollmorgen Space cannot communicate with the drive while a different than standard settings are used. Set U0 dip OFF to communicate with the PC again or use the Service Serial Communication. |